Sideloop Interlock Binary to Binary - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
This module passes the enumerated value (typically from a Binary Input) to an enumerated output (typically connect to a Binary Output). The value may be delayed based on the selected delay type (None, On, Off, or Both.)

You can view and modify the modules in this group’s logic.

The Sideloop Interlock Binary to Binary modules work with the state selection mode (optional).

To see a module's connections and how modules interact with it, view the Connections table.