Attributes (Sideloop Interlock Binary to Analog) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The following table describes the attributes used by the Sideloop Interlock Binary to Analog module.

Table 1. Sideloop Interlock Binary to Analog Attributes

Name

Type 1

Description

Default Value

Input

 

Contains the input to this module.

Off

Set Name: Off/On

Mode

 

Contains a connection to the Selection object of a control System. It overrides the internal logic.

Control

Set Name: Off/On/Control

Present Value

G, V

Analog value output based on the input and the status of the associated delays.

 

SL-DELAYTYPE (Delay Type)

 

Selects the type of delay from the time the binary input is energized or de-energized to the time when the analog output goes to Output Range High or Output Range Low. This can be set for None, On, Off, or Both.

None

Set Name: BI to BO/AO Delay Type

SL-OFFDELAY (Off Delay)

 

Specifies the delay from the time the input is de-energized to the time when the analog output goes to Output Range Low.

30 Seconds

SL-ONDELAY (On Delay)

 

Specifies the delay from the time the binary input is energized to the time when the analog output goes to Output Range High

30 Seconds

SL-OUTA (Output Range Low)

 

Contains the value sent to the output when the input is off and all timers are satisfied. If the Mode is Off, this value is sent to the Output.

0.0

SL-OUTB (Output Range High)

 

Contains the value sent to the output when the input is on and all timers are satisfied. If the Mode is On, this value is sent to the Output.

100.0

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)