Reliability (Sequencer) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
  • The reliability associated with the Sequencer module may report the input unreliable. When the input is unreliable, all outputs hold the last value set when the input was reliable during this situation.

  • If the Sequencer is unable to stage up or down because the remaining outputs are disabled, the Sequencer’s reliability is Unreliable.