Attributes (Pass Through) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The following table describes the attributes used by the Pass Through (Enum) modules.

Table 1. Pass Through (Enum) Attributes

Name

Type 1

Description

Default Value

Input

 

The input to the pass through module.

1st Enum or False

Present Value

G, V

The output of the pass through module

 
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)