Reliability (Global Sequencer) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
  • The reliability associated with the Global Sequencer module may report Input Unreliable. This condition occurs when an Input is unreliable. When it is unreliable, all outputs hold the last value set when all inputs are reliable.

  • If the Global Sequencer is unable to stage up because the remaining outputs are disabled, the Global Sequencer’s reliability remains Reliable, but the Global Sequencer object Status and Operating State attributes change to Insufficient Capacity.