Lighting - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Lighting Control module provides lighting operation. It accepts a two-state enumerated input and outputs a two-state enumerated Present Value. The Present Value typically is sent to a Binary Output object that controls the physical lighting hardware. For Pulse type lighting outputs, the Lighting Control module monitors the Light Status input and changes (if necessary) the Polarity output to synchronize the lighting hardware with the desired Present Value.

You cannot view or modify the modules in this group’s logic.