Reliability (Heating Sequenced Valves with Low Limit) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English
Table 1. Heating Sequenced Valves with Low Limit Reliability

Input

Behavior When Input Is Not Reliable

OA Temperature

If the requested mode is Low OA Temperature, the output controller changes to Failsoft.

Low Limit Process Variable

If the requested mode is Remain In Control, the output controller changes to Failsoft.