Module Use in Applications (Heating Proportional Output with Enable) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Heating Proportional Output with Enable Uses in Application System Selection Trees
Module Instance Name Applications
Heating Proportional Output with Enable VAV Single Duct Applications

VAV Subordinate Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.