Reliability (Heating Proportional Valve with Low Limit) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Table 1. Heating Proportional Valve with Low Limit Reliability

Input

Behavior When Input Is Not Reliable

Low Limit Process Variable

If the requested mode is Remain In Control, the output controller changes to Failsoft.

OA Temperature

If the requested mode is Low OA Temperature, the output controller changes to Failsoft.