Module Use in Applications (Heat Recovery Wheel with Bypass Dampers) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Heat Recovery Wheel with Bypass Dampers Uses in Application System Selection Trees

Module Instance Name

Applications

Heat Exchanger with Bypass Dampers

AHU Mixed Air Single Duct Applications

AHU 100% Outdoor Air Single Duct Applications

Heat Recovery Wheel with Bypass Dampers v50

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications

AHU 100% Outdoor Air Single Duct Applications

AHU 100% Outdoor Air Dual Duct Applications

AHU Multizone (Mixed Air Dual Duct) Applications

To see a module's connections and how modules interact with it, view the Connections table.