Module Use in Applications (Heat Pump Staged Compressors) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Heat Pump Staged Compressors Uses in Application System Selection Trees

Module Instance Name

Applications

Staged Compressor Control v51

Heat Pump Applications

To see a module's connections and how modules interact with it, view the Connections table.