Module Use in Applications (Cooling Staged Outputs with Dehumidification) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Cooling Staged Outputs with Dehumidification Uses in Application System Selection Trees

Module Instance Name

Applications

AHU Staged Cooling Control v50

All

To see a module's connections and how modules interact with it, view the Connections table.