Module Use in Applications (Cooling Proportional Valve) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The application System Selection trees use the individual modules in this group using the names the following table.

Table 1. Cooling Proportional Valve Uses in Application System Selection Trees

Module Instance Name

Applications

Proportional Cooling Control v51

Fan Coil Applications

Unit Ventilator Applications

To see a module's connections and how modules interact with it, view the Connections table.