Module Use in Applications (Single Speed Fan Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Single Speed Fan Control Uses in Application System Selection Trees

Module Instance Name

Applications

Single Speed Fan Control

Fan Coil Applications

Heat Pump Applications

Unit Ventilator Applications

To see a module's connections and how modules interact with it, view the Connections table.