Fan Supply Duct Static Control - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This module is designed to use the supply fan to control the supply air duct static pressure. The module has inputs for the desired mode, a ramp rate, pressure, pressure setpoint, and process units. The module is also designed to accept commands from a FSCS. The FSCS input takes precedence over the mode input.