Primary States (Fan Single Speed) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
  • Off: Turn the fan off. The Fan OnOff is set to Off.

  • On: Turn the fan on. The Fan OnOff is set to On.

  • Hold: The fan remains in the state it was in when this mode was requested. If it is on, it stays on. If it is off, it stays off.