Attributes (Fan Single Speed) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The following table describes the attributes used by the Fan Single Speed modules.

Table 1. Fan Single Speed Attributes

Name

Type 1

Description

Default Value

Fan OnOff

 

Contains the output command enumeration for information feedback representing the on/off status of the fan.

Set Name: Off/On

FAN-OUTSTATE (State)

 

Current operational state of the output controller.

Set Name: Off/On/Hold

Mode

 

Mode requested by State Selection.

Off

Set Name: Off/On/Hold

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)