Fan Return or Exhaust BSP Control - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Return Fan BSP module controls a variable speed fan and building static pressure (BSP) in an air handler application. This module accepts building static pressure, and setpoints. The module has outputs for controlling a variable speed return fan.