Module Use in Applications (Dual Fan Run-Standby) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Dual Fan Run-Standby Uses in Application System Selection Tree

Module Instance Name

Application

Dual Exhaust Fan Run-Standby

AHU 100% Outdoor Air Single Duct Applications

Dual Relief Fan Run-Standby

AHU Mixed Air Single Duct Applications

Dual Return Fan Run-Standby

AHU Mixed Air Single Duct Applications

Dual Supply Fan Run-Standby

AHU Mixed Air Single Duct Applications

AHU 100% Outdoor Air Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.