Attributes (Device OR) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The following table describes the attributes used by these modules.

Table 1. Device OR Attributes

Name

Description

Default Value

Device 1 OnOff Indicates binary status of device 1. Off
Device 2 OnOff Indicates binary status of device 2. Off
Alarm OR If any input is on, this output is on. Off