Device OR - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

This module is responsible for examining two enumeration inputs and provides OR logic where at least one input must be On for the output to be On. The module accepts two Off/On inputs and has a output.