The following table describes the attributes used by these modules.
Name |
Description |
Default Value |
---|---|---|
Damper isAvailable | Indicates the availability of the damper. | True |
Damper OpenClose | Provides the control signal output to the damper BO. | Close |
Damper Status | Indicates the status of the commanded damper. | Open |
Delay | Indicates the time required to wait before starting the fan when the mode is On, and alternatively close the dampers when the mode is Off. | 60.0 seconds |
Fan OnOff | Provides the control signal output to the fan BO. | Off |
Fan Status | Indicates the status of the commanded fan. | Off |
Mode | Indicates the required fan command. | Off |
State | Represents the current state of the hybrid activity. | Off |