Module Use in Applications (Damper Control with Low Limit) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Damper Control with Low Limit Uses in Application System Selection Trees

Module Instance Name

Applications

Proportional Damper Output v51

Heat Pump Applications

Proportional Unit Vent 3 Damper Control v51

Unit Ventilator Applications

To see a module's connections and how modules interact with it, view the Connections table.