VF Primary Min Flow Control - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This module controls a proportional source within a control application. The module accepts a mode, a process variable, and a setpoint as inputs. Based upon the input mode and parameter settings, the module outputs a percent command and control status. This module resets the PIDs to default tuning parameters if the Reset PID Tuning input is true. This module is implemented as a standard Control Activity.

You can view and modify the modules in this group’s logic.