Attributes (Sequenced Output) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The following table describes the attributes used by the Sequenced Output modules:

Table 1. Sequenced Output Attributes

Name

Type 1

Description

Default Value

Input (Float)

 

Provides the variable that comes from the PID that is spanned across two outputs.

0%

Valve 1 Percent Capacity

 

Indicates the capacity of the first valve, in percent.

33.3%

Valve 1 Percent Cmd

V

Provides an output from the span.

0%

Valve 2 Percent Cmd

V

Provides an output from the span.

0%

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)