Sequenced Output - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The Sequenced Output module takes one proportional output and spans it over two proportional outputs. This module accepts as inputs an Input (float) and a Valve 1 Percent Capacity. Based on the input commands, the module outputs two proportional outputs.

You can view and modify the modules in this group’s logic.