Module Use in Applications (Secondary Pump PID) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Secondary Pump PID Uses in Application System Selection Trees

Module Instance Name

Applications

Secondary Bypass Valve PID v50

Central Cooling Applications

Central Heating Applications

Secondary Chill Water Pump PID v50

Central Cooling Applications

Secondary Hot Water Pump PID v50

Central Heating Applications

To see a module's connections and how modules interact with it, view the Connections table.