Module Use in Applications (Pump Selector) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Pump Selector Uses in Application System Selection Trees

Module Instance Name

Applications

CWP Selector XX (Where XX Is 01-08)

Central Cooling with Optimization Applications

PCHWP Selector XX (Where XX Is 01-08)

Central Cooling with Optimization Applications

Pump Selector XX (Where XX Is 01-08)

Central Cooling with Optimization Applications

SCHWP Selector XX (Where XX Is 01-08)

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.