The following table describes the attributes used by the Pump Output Control modules:
Attribute |
Type 1 |
Description |
Default Value |
---|---|---|---|
Blocking Protect |
This input is the signal from blocking protection. When this input is Protect, the device turns on for few seconds once a week. |
Off Set Name: Blocking Protect |
|
Command |
This input is the command to the device. The input usually comes from the device sequencer. |
False |
|
Device OnOff |
V |
This output provides the on-off signal to turn the pump on and off. |
Default Value: Off Set Name: Off/On |
Enable |
This input is the status of the enable for this pump. |
True |
|
Min Speed |
This input is the minimum value of the Percent Command when the Percent Cmd is equal or less than Min Speed. |
0.0% |
|
Percent Cmd |
V |
This input is the value from the static pressure control PID module. It provides the control signal for the VFD outputs. |
0.0% |
Percent Command |
V |
This output is the percent command that is being sent to the Variable Frequency Drive (VFD) for the pump. |
Default Value: 0.0 Display Units: % |
Percent Limit |
This input is the maximum value of the Percent Command when the Percent Cmd is equal or greater than Percent Limit. |
100.0% |
|
Ramp Time |
This input is the time (in minutes) for the module to ramp from zero to the minimum of the Percent Limit and the Percent Cmd on startup. |
5.0 Minutes |
|
Speed Setting |
This input indicates whether the controlled device is variable speed or constant speed. |
Constant Capacity Set Name: AHU Supply Fan Type |
|
State |
G |
This is the current state of the activity. |
Default Value: Off Set Name: CP Pump Output Control |
System Enable |
This input indicates that the chilled water system is enabled. |
True |