Module Use in Applications (Pump Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Pump Control Uses in Application System Selection Trees

Module Instance Name

Applications

CW Pump X Control v2 (Where X Is 1-8)

Central Cooling Applications

Primary CHW Pump X Control v2 (Where X Is 1-8)

Central Cooling Applications

Primary Pump X Control v2 (Where X Is 1-8)

Central Heating Applications

Secondary CHW Pump X Modulating Control v2 (Where X Is 1-8)

Central Cooling Applications

Secondary HW Pump X Control v2 (Where X Is 1-8)

Central Heating Applications

To see a module's connections and how modules interact with it, view the Connections table.