Primary States (Heat Exchanger with Return Water Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
  • Off: Set the Percent Request and Percent Cmd to 0%.

  • Max: Set the output to maximum. Set the Percent Request and Percent Cmd to 100%.

  • Control: Adjust the output to control the Process Variable. If the leaving heating source water temperature drops below the limit, the control valve opens further to control the leaving water temperature.