The following table describes the attributes used by the Hx Selector modules:
Name |
Description |
Default Value |
---|---|---|
CHW Commanded Flow |
Indicates the actual chilled water flow based on the pump status and pump ratings. This value is used in the percent load calculations for headered CHW systems only, and is typically available from the CHW Pump Selector. The Flow Stabilize Timer starts when the CHW Commanded Flow changes, and has a duration of 0.2 * Stabilize Time. This timer prevents the changes of the Process Variable from being recognized, and allows the system to stabilize following a change in the headered CHW flow. |
0 Display units come from Flow Units. Minimum Value: 0 |
CHW Headered/ Dedicated |
Specifies whether operating with headered, dedicated, or no pumping on the Chilled Water side of the heat exchanger. |
Headered Set Name: Headered Dedicated |
Control Mode |
Determines how the process variable is treated:
|
Building Load Set Name: Hx Control Mode |
CW Commanded Flow |
Indicates the actual condenser water flow based on the pump status and pump ratings. This value is used in the percent load calculations for headered CW systems only, and is typically available from the CW Pump Selector. . |
0 Display units come from Flow Units. Minimum Value: 0 |
CW Headered/ Dedicated |
Specifies whether operating with headered, dedicated, or no pumping on the Condenser Water side of the heat exchanger. |
Headered Set Name: Headered Dedicated |
Derate Now |
Enables Derate Now, which commands the Hx Selector module to calculate a reduced capacity of the running heat exchangers and then command the module to reevaluate which heat exchangers should be operating. |
False |
Derate Reset |
Resets the Derating Percent back to zero instantly. |
False |
Derating Percent |
Indicates the percentage of derating internally applied to all devices. This value is calculated and used in Building Load Mode only. If devices are unable to meet the rated capacities, elsewhere in the application the Derate Now input is set to True. The Hx Selector then derates the devices by this percentage. Large values of this property should be investigated since it could indicate possible malfunction of the heat exchangers. |
0 Display Units: % |
HX AVAILABLE CAP |
Indicates the sum of the enabled derated capacities. |
0
Display Units: Tons |
HX BASE LOAD |
Indicates the minimum rate cooling the heat exchanger selector maintains. |
0.1
Display Units: Tons |
HX CURRENT CAP |
Indicates sum of the derated capacities of the devices currently commanded on. |
0
Display Units: Tons |
HX CURRENT PCT LOAD |
Indicates the percent loading of the devices currently commanded on, adjusted by the Derating Percent. |
0
Display Units: % |
HX-MINOFFTIME (Min Off Time) |
Indicates the minimum amount of off time applied to all devices. |
10 Display Units: Min Range: 1-120 |
HX-MINONTIME (Min On Time) |
Indicates the minimum amount of on time applied to all devices. |
10 Display Units: Min Range: 1-120 |
HX START DELAY (System Start Delay)b |
Indicates the delay applied when the System Enabled input transitions from Disabled to Enabled. The Minimum Load is maintained during this time, allowing the chilled and condenser water pumps to operate. This time period is typically longer than the Stabilize Time to allow the system to achieve steady state after not being under control for some time. |
30 Display Units: Min |
HX1-REQUIRED DEVS (Required Devices) |
Provides an integer output representing the packed bits of the desired steady state set of devices commanded On. For example, a value of 88 means 0-1-0-1-1-0-0-0, which indicates device 2, 4, and 5 are On, and the rest are Off. |
0 |
HX1-REQD INTERIM DEVS (Required Interim Devices) |
Provides an integer output representing the packed bits of the intermediate devices requested to turn on while the heat exchanger selector moves toward the desired steady state. |
0 |
Iso Valve Stroke Time |
Indicates stroke time of the isolation valves. This input delays turning on the first headered pumps. For dedicated pumping on both CW and CHW sides, this value should equal zero. |
60 Display Units: Sec |
Max CHW Flow |
Indicates the sum of the Rated CHW Max Flows of all the devices currently On. |
0 Display units come from Flow Units. |
Min CHW Flow Setpoint |
Indicates the minimum flow required for safe chiller operation. This output is used in headered variable speed chilled water systems. |
0 Display units come from Flow Units. |
Min CW Flow Setpoint |
Indicates the minimum flow required for safe chiller operation. This output is used in headered variable speed condenser water systems. |
0 Display units come from Flow Units. |
Process Variable Units |
Indicates the units used for the Process Variable depending on the Units of the application and the Mode of Operation. |
kW Set Name: Unit |
Pump Delay |
Indicates the longest amount of time required for the pump to stop once a stop is received, or the amount of time to speed up once the on command is received. |
15 Display Units: Sec Range: 0-120 |
Pump Down Timeb |
Indicates the amount of time to run the CW and CHW pumps after turning off a device. This delay allows the removal of refrigerant from the evaporator. |
10 Display Units: Min Range: 1-120 |
Required CHW Flow |
Indicates the required chilled water flow associated with the currently requested (or soon to be requested) devices. This output is used in headered chilled water systems. To ensure enough chilled water flow during taging, the CHW Required Flow is increased by 10% with a minimum value as calculated and a maximum value equal to the Rated CHW Flow. This flow requirement value is issued with enough anticipation to allow flows to be obtained prior to devices turning on and maintains its high value while the Pump Down Timer is active, when devices are being turned off. |
0 Display units come from Flow Units. |
Required CW Flow |
Indicates the required condenser water flow associated with the currently requested (or soon to be requested) devices. This output is used in headered condenser water systems. The module calculates a minimum condenser water flow based on the individual minimum condenser water requirements and the rated condenser water flows. To ensure enough condenser water flow during staging, the CW Required Flow is increased by 10% with a minimum value as calculated and a maximum value equal to the Rated CW Flow. This flow requirement value is issued with enough anticipation to allow flows to be obtained prior to devices turning on and maintains its high value while the Pump Down Timer is active, when devices are being turned off. |
0 Display units come from Flow Units. |
Required Tower Flow |
Indicates the required cooling tower water flow. This output is a time-shifted version of the Required CW Flow output to ensure proper sequencing of the cooling tower with the other equipment when devices are added or removed. |
0 Display units come from Flow Units. |
Rotate Now |
On the rising edge of this signal, the Hx Selector calculates a new combination of devices that provides the required cooling capacity while promoting the maximum rotation of the heat exchanger. |
False |
Rotation Mode |
Determines how rotation is processed:
|
None Set Name: Rotation Mode |
Selector Enabled |
Indicates if Heat Exchanger is in operation. This input enables Heat Exchanger to determine if it can turn on pumps before opening its first isolation valves (turning on the first heat exchanger) or close its last isolation valves before turning off all the pumps (turning off the last heat exchanger). This input connects to the same source as Chiller Selector's System Enabled input, if present. |
False |
Sequence Row Control |
Enables Sequence Row parameter to enable devices. |
False |
Sequence Row |
Indicates the sequence table row number that the module attempts to move toward while following device timers and statuses. This input is available when the Sequence Row Control input is True. If the input value is out of range or if a sequence table is not present, Sequence Row input is ignored. |
0 |
Stabilize Time |
Indicates the amount of time after a device changes on or off that the must elapse before recognizing changes to the Process Variable. |
15 Display Units: Min Range: 15-120 |
System Enabled |
Disables/enables the chiller plant. When System Enabled is False, the Heat Exchanger Selector downstages to zero capacity. |
False |
Tower Available Flow |
Indicates the available cooling tower water flow. The Hx Selector uses this value in determining valid device combinations. The value is typically available from the Cooling Tower Selector. |
0 Minimum Value: 0 Display units come from Flow Units. |
Tower Commanded Flow |
Indicates the actual cooling tower water flow. This value provides status feedback to the Hx Selector to ensure proper sequencing of the cooling tower with the other equipment when a device is added or removed. The value is typically available from the Cooling Tower Selector. |
0 Minimum Value: 0 Display units come from Flow Units. |
Tower Piping |
Specifies whether operating with headered, dedicated, or no cooling tower piping on the Condenser Water side of the heat exchanger. |
Headered Set Name: HeaderedDedicated |