Module Use in Applications (Cooling Tower Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection Trees use the individual modules in this group using the names in the following table.

Table 1. Cooling Tower Control Uses in Application System Selection Trees

Module Instance Name

Application

Cooling Tower X Control (Where X is 1-8)

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.