Cooling Tower Control - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Cooling Tower Control module coordinates the outputs to a cooling tower. This module supports single speed, two speed, three speed, or variable speed tower fans.

The module accepts a percent command, speed commands, and an isolation valve command to determine which outputs are active. When the fans are multi-speed, this module ensures that only the currently required speed output is active.

For information on how the FSM determines the state, see FSM (Fan Speed).

Figure 1. Cooling Tower Control