The following table describes the attributes used by the Chiller Selector modules:
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Available Capacity |
V |
Provides the sum of the derated capacities of the enabled devices. |
0 Display units come from Capacity Units. |
CHLR CAP LIMIT (Capacity Limit) |
V |
Limits the capacity of the devices currently on for a time to achieve a more stable transition when adding a device. This output is used in headered chilled water systems with variable speed chillers only. You may set up the Capacity Limit feature in Manual or Automatic mode using the Capacity Limit Setup input:
|
100 Display Units: % Range: 30-100 |
Capacity Limit Hold Time |
Indicates the amount of time to restrict the output when Capacity Limit is active. |
10 Display Units: Min Minimum Value: 1 Maximum Value: Less than Stabilize Time |
|
Capacity Limit Setup |
Determines the Capacity Limit feature implementation. The options are Manual or Automatic. |
Manual Set Name: Reset Type |
|
CHLR CURRENT LIMIT (Capacity Limit User Input) |
Limits the total capacity of all devices currently on when the Capacity Limit Setup is Manual and Capacity Limit is active. |
60 Display Units: % Range: 30-100 |
|
Capacity Units |
Indicates the units used for capacity depending on the Units of the application. |
Tons Set Name: Unit |
|
CHW Available Flow |
Indicates the chilled water flow available based on the pump enables and pump ratings (for headered CHW systems). Chiller combinations requiring a minimum headered chilled water flow greater than this value are not requested. This value is typically available from the CHW Pump Selector. |
0 Display units come from Flow Units. Minimum Value: 0 |
|
CHW Commanded Flow |
Indicates the actual chilled water flow based on the pump status and pump ratings. This value is used in the percent load calculations for headered CHW systems only, and is typically available from the CHW Pump Selector. This value must be greater than CHW Min flow defined in the Device Info Table before the chiller can be commanded on. |
0 Display units come from Flow Units. Minimum Value: 0 |
|
CHW Headered/Dedicated |
Specifies whether operating with headered, dedicated, or no pumping on the Chilled Water side of the chiller. |
Headered Set Name: HeaderedDedicated |
|
CHW Iso Valve/Pump nn Cmd |
V |
Provides the request commands to the chilled water side isolation valves or any dedicated pumps (where nn is 01-08). Headered pumps are not controlled by this module. |
False |
CHW Max Flow |
Indicates the maximum chilled water flow of each device. |
0 Display units come from Flow Units. |
|
CHW Min Flow |
Indicates the minimum chilled water flow of each device (in flow units). |
0 Display units come from Flow Units. |
|
CHW Temperature |
Provides the Chilled Water Temperature input, which is used to calculate the instantaneous Uprated Capacity of the devices. |
6.7 °C, 44 °F Minimum: 18 °C, 0 °F Maximum: 50 °C, 120 °F |
|
CHLR COAST (Coast) |
Allows the module to stage down when the load diminishes, by turning off devices (instead of switching to smaller devices) while preventing the module from staging up even if the load increases. |
False |
|
Control Mode |
Determines how the process variable is treated:
|
Building Load Set Name: Chiller Control |
|
Current Capacity |
G, V |
Provides the sum of the derated capacities of the devices currently on (that is, Device nn Status = On). |
0 Display units come from Capacity Units. |
Current COP |
V |
Indicates the capacity weighted efficiency (COP) of the devices currently commanded to On. |
0.1 Display Units: % |
Current Percent Load |
V |
Indicates the percent loading of the devices currently commanded to On adjusted by the Derate Percent. |
0 Display Units: % |
Current/Power Units |
Indicates the units used for the current/power depending on the Units of the application. |
A Set Name: Unit |
|
CW Available Flow |
Indicates the condenser water flow available based on the pump enables and pump ratings (for headered CW systems). Chiller combinations requiring a minimum headered condenser water flow greater than this value are not requested. This value is typically available from the CW Pump Selector. |
0 Display units come from Flow Units. Minimum Value: 0 |
|
CW Commanded Flow |
Indicates the actual condenser water flow based on the pump status and pump ratings. This value is used in the percent load calculations for headered CW systems only, and is typically available from the CW Pump Selector. This value must be greater than CW Min flow defined in the Device Info table before the chiller can be commanded on. |
0 Display units come from Flow Units. Minimum Value: 0 |
|
CW Headered/Dedicated |
Specifies whether operating with headered, dedicated, or no pumping on the Condenser Water side of the chiller. |
Headered Set Name: HeaderedDedicated |
|
CW Iso Valve/Pump nn Cmd |
V |
Provides the request commands to the condenser water side isolation valves or any dedicated pumps (where nn is 01-08). Headered pumps are not controlled by this module. |
False |
CW Min Flow |
Indicates the minimum condenser flow of each device (in flow units). |
0 Display units come from Flow Units. |
|
CW Temperature |
Provides the Condenser Water Temperature input, which is used to calculate the instantaneous Uprated Capacity of the devices. |
29.4 °C, 85 °F Minimum: 2 °C, 35 °F Maximum: 50 °C, 120 °F |
|
Delta Temperature Units |
Indicates the units used for temperature depending on the Units of the application. |
delta °F Set Name: Unit |
|
Derate Now |
Forces an upstage. This input is used only when the Control Mode is Building Load, as possible device malfunction (for example, a fouled device or a day that is beyond the design day) may result in not meeting the building load, and the module is unable to determine a saturation condition from the input Process Variable or the calculated percent load. The module acts as it is meeting the cooling demand. Therefore, this input may force a necessary upstage. |
False |
|
Derate Reset |
Resets the derating percent value to zero instantly rather than waiting for its inherent decay. The derate reset action is triggered at the rising edge of the module. See Derate Now. |
False |
|
Derating Percent |
V |
Indicates the percentage of derating internally applied to all devices. This value is calculated and used in Building Load Mode only. If devices are unable to meet the rated capacities, elsewhere in the application the Derate Now input is set to True. The Chiller Selector then derates the devices by this percentage. Large values of this property should be investigated since it could indicate possible malfunction of the chillers. |
0 Display Units: % |
Device Info |
Provides a structure of arrays containing individual information of each device. This structure contains: Rated Capacity, CW Min Flow, Rated CW Flow, CHW Min Flow, Rated CHW Flow, Peak COP, Device Lift, Lift Sensitivity, Rated Current/Power, CHW Max Flow, Max Pct Load, Min Pct Load, Min Pct Load COP, Max Pct Load COP, Interstage Transition Delay, Stabilize Time. |
||
Lift Sensitivity |
Indicates the sensitivity of the device capacity to changes in the difference between the condenser and chilled water temperatures. The Chiller Selector adjusts the capacity due to lift according to the following equation: Ca = S * (La - Lr) + Cr where:
S is calculated as follows: S = (Ca - Cr) / (La - Lr) |
0.0 Units: kW, °C, Ton, °F |
|
Device nn Cmd |
V |
Provides the lift request commands to each device (where nn is 01-08). |
False |
Device nn Current Power Out |
V |
Provides an output with the Rated Capacity used elsewhere in the application (where nn is 01-08). |
0 Display units come from Capacity Units. |
Device nn Enable |
Indicates the Disable/Enable state of the devices (where nn is 01-08). |
True |
|
Device nn Runtime |
Indicates the runtimes of the devices (where nn is 01-08). |
0 Display Units: Hours |
|
Device nn Start Count |
Indicates the number of starts performed by each device (where nn is 01-08). |
0 |
|
Device nn Status |
Indicates the current Off/On state of the devices as reported by the hardware itself (where nn is 01-08). |
Off Set Name: Off/On |
|
Device Type |
Indicates the required letter for each device. If the types are all the same or it doesn’t matter, then use Type A for each. The default value is all devices Type A. |
Type A Set Name: Chiller Type |
|
Flow Units |
Indicates the units used for the flow depending on the Units of the application. |
gpm Set Name: Unit |
|
Hysteresis |
Indicates the value of an additional efficiency penalty to be applied before a change is made. Larger values increase the stability of the chiller combination currently operating while forcing a greater drop in efficiency before a switch is made. The adjusted efficiency of the new combination includes this Hysteresis. |
0.005 Display Units: % |
|
Interstage Off Delay |
Delay after an Off command before starting to downstage again. |
0.1 Display Units: Min Range: 0.1-10.0 |
|
Interstage On Delay |
Delay after an On command before starting to upstage again. |
15 Display Units: Min Range: 0.1-120 |
|
Interstage Transition Delay |
When changing from one combination of devices to another, this is the amount of time to wait between turning one device on and another device off. For example: The system has three chillers, and chillers 1 and 3 are running, and the system requirements change such that it is more efficient to run chillers 1 and 2. This scenario requires two chillers to change and only one is allowed to change at a time. Therefore, the chiller selector turns on chiller 2, waits the interstage delay time, then turns off chiller 3. |
8 Display Units: Min Range: 1-120 |
|
Is Stable |
SC, V |
Specifies whether the Stabilize Timer has expired and the Process Variable can be used to update the combination of devices. The stabilize timer starts when a chiller command output or a chiller status input changes. A shorter stabilize timer (20% of the Stabilization Time) also starts when the Chilled Water Commanded Flow input changes due to the start or stop of a chilled water pump. |
False |
Iso Valve Stroke Time |
Indicates the stroke time of the isolation valve. This input delays the process of turning the chilled water pump on and off. Since dedicated systems do not use this type of valve, the tool sets this property equal to zero during selection. |
60 Display Units: Sec Range: 0-180 |
|
CHLR LOWER PCT LOAD (Lower Optimal Pct Load) |
Indicates the left hand endpoint of the chiller efficiency plateau. When the percent load goes below this value, the module considers other combinations of devices that would produce a higher percent load. This is a nominal value that applies to each device individually. |
60 Display Units: % The maximum value must be less than the Higher Optimal Pct Load value. Minimum Value: 30 |
|
Low Load |
Indicates the only operating chiller has been commanded off to provide chilled water more efficiently. |
False |
|
Max CHW Flow |
Indicates the sum of the Rated CHW Max Flows of all the devices currently On. This is the maximum amount of variable speed CHW Flow that the chiller selector is allowing the Variable Speed Pump Selector to command. |
0 Display units come from Flow Units. |
|
Max Delta CHWT |
Indicates the maximum temperature drop across all devices in selectable units. This value is used when the Control Mode is Temperature Differential. When the process variable (Temperature Differential) equals this value, the percent loading is 100%. |
12 Display units come from Delta Temperature Units. |
|
Min CHW Flow Setpoint |
V |
Indicates the minimum flow required for safe chiller operation. This output is used in headered variable speed chilled water systems. |
0 Display units come from Flow Units. |
Min CW Flow Setpoint |
V |
Indicates the minimum flow required for safe chiller operation. This output is used in headered variable speed condenser water systems. |
0 Display units come from Flow Units. |
CHLR-MINOFFTIME (Min Off Time) |
Indicates the minimum amount of off time applied to all devices. |
10 Display Units: Min Range: 1-480 |
|
CHLR-MINONTIME (Min On Time) |
Indicates the minimum amount of on time applied to all devices. |
10 Display Units: Min Range: 1-480 |
|
CHLR BASE LOAD (Min Required Capacity) |
Indicates a value in units of load. The Chiller Selector module maintains, at a minimum, this amount of rated cooling. It is recommended to set this input to the desired chiller capacity times the optimal percent load (halfway between the lower and upper optimal percentages). For example, if the average of the Upper and Lower Optimal Load Percent is 80% and the minimum run conditions are two 70T chillers, the Min Required Capacity is (2 * 70) * 80% = 112T. |
0.1 Display units come from Capacity Units. The minimum value must be greater than 0. |
|
Peak COP |
Indicates the peak Coefficient of Performance (COP) of each device, which is the ratio of cooling output to power input. Combinations of devices that have higher peak COPs are preferentially selected during operation without regard for improving run time or start count imbalances. Only devices with the same Peak COP have the ability to be balanced for run time and/or start counts. For example, if two devices have peak COPs X and two other devices have peak COPs Y, start count and runtime balancing occurs among the devices with peak COPs X and among the devices with peak COPs Y but not among all devices. This happens because the run time and start count adjustments are an order of magnitude more precise (to the hundredths place) than the precision of the Peak COPs (to the tenths place). |
7.0 Minimum Value: 0.1 Display Units: % |
|
Predicted Adjust COP |
SC, V |
Indicates the Predicted COP adjusted for runtime, start count, start/stop, load change, and hysteresis penalties. |
0.1 |
Predicted COP |
SC, V |
Indicates the expected capacity weighted coefficient of performance (COP) based on the Required Devices (steady state device commands). |
0.1 Display Units: % |
Predicted Percent Load |
SC, V |
Indicates the expected percent load based on the Required Devices (steady state device commands). |
0 Display Units: % |
Process Variable |
Provides a value used to determine the current load of the chiller plant. See Control Mode. |
0 Display units come from Process Variable Units. When Mode is Building Load, Chiller Load, or Temperature Differential, the minimum value is 0. |
|
Process Variable Units |
Indicates the units used for the Process Variable depending on the Units of the application and the Mode of Operation. When the Mode is Chiller Load, an selection option is available in the System Selection wizard. |
kW Set Name: Unit |
|
Pump Delay |
Indicates the longest amount of time required for the pump to stop once a stop is received, or the amount of time to speed up once the on command is received. |
15 Display Units: Sec Range: 0-120 |
|
CHLR PMP DWN TIME (Pump Down Time)b |
Indicates the amount of time to run the CW and CHW pumps after turning off a device. This delay allows the removal of refrigerant from the evaporator. |
10 Display Units: Min Range: 1-120 |
|
Rated Capacity |
Indicates the cooling capacities of each device (in capacity units). |
0 Display units come from Capacity Units. |
|
Rated CHW Flow |
Indicates the rated chilled water flow of each device (in flow units). |
0 Display units come from Flow Units. |
|
Rated CHW Max Flow |
Indicates the rated maximum flow of each device (in flow units). |
0 Display units come from Flow Units. |
|
Rated Current Power |
Indicates the rated current of each device. |
0 Display units come from Current/Power Units. |
|
Rated CW Flow |
Indicates the rated condenser flow of each device (in flow units). |
0 Display units come from Flow Units. |
|
Required CHW Flow |
V |
Indicates the required chilled water flow associated with the currently requested (or soon to be requested) devices. This output is used in headered chilled water systems. To ensure enough chilled water flow during chiller staging, the CHW Required Flow is increased by 10% with a minimum value as calculated and a maximum value equal to the Rated CHW Flow. This flow requirement value is issued with enough anticipation to allow flows to be obtained prior to devices turning on and maintains its high value while the Pump Down Timer is active, when devices are being turned off. |
0 Display units come from Flow Units. |
Required CW Flow |
V |
Indicates the required condenser water flow associated with the currently requested (or soon to be requested) devices. This output is used in headered condenser water systems. The module calculates a minimum condenser water flow based on the individual minimum condenser water requirements and the rated condenser water flows. To ensure enough condenser water flow during chiller staging, the CW Required Flow is increased by 10% with a minimum value as calculated and a maximum value equal to the Rated CW Flow. This flow requirement value is issued with enough anticipation to allow flows to be obtained prior to devices turning on and maintains its high value while the Pump Down Timer is active, when devices are being turned off. |
0 Display units come from Flow Units. |
Required Devices |
SC, V |
Provides an integer output representing the packed bits of the desired steady state set of devices commanded On. For example, a value of 88 means 0-1-0-1-1-0-0-0, which indicates device 2, 4, and 5 are On, and the rest are Off. |
0 |
Required Interim Devices |
SC, V |
Provides an integer output representing the packed bits of the intermediate devices requested to turn on while the chiller selector moves toward the desired steady state. |
0 |
Required Tower Flow |
V |
Indicates the required cooling tower water flow. This output is a time-shifted version of the Required CW Flow output to ensure proper sequencing of the cooling tower with the other equipment when devices are added or removed. This is the sum of the chiller rated flow sent to the cooling tower selector. |
0 Display units come from Flow Units. |
Rotate Now |
On the rising edge of this signal, the Chiller Selector calculates a new combination of devices that provides the required cooling capacity while promoting the maximum rotation of the chillers. |
False |
|
Rotation Mode |
Determines how rotation is processed:
|
None Set Name: Rotation Mode |
|
Sequence Row |
Indicates a sequence table row number that the module attempts to move toward while following device timers and statuses. This input is available when the Sequence Row Control input is True. If the input value is out of range or if a sequence table is not present, Sequence Row input is ignored. |
0 |
|
Sequence Row Control |
Enables Sequence Row parameter to enable devices. |
False |
|
Sequence Table |
Provides an array of integers. Each column is a device type letter (maximum of letter types above). Each row is a combination represented by counts of each device type. |
||
Stabilize Time |
Indicates the amount of time after a device changes on or off that the must elapse before recognizing changes to the Process Variable. |
15 Display Units: Min Range: 15-120 |
|
Staging Margin |
When considering a downstage combination, the percent load actually increases by this value when performing the efficiency calculation. This method provides a safety margin as the percent load is a theoretical value, and the actual percent load of the new combination could be higher than calculated. When considering an upstage combination, the percent load actually reduces by this value when performing the efficiency calculation. This method provides a safety margin as the actual percent load of the new combination could be lower than calculated. Since the Upper Optimal Pct Load is typically closer to 100% than the Lower Optimal Pct Load is to 0%, the slope of the right hand side curve is much steeper than the left hand side slope; therefore, when the load is increasing, the system efficiency of the current combination drops faster compared with the slower increase of efficiency of the new combination, allowing the algorithm to switch to a new stage. |
2.0 Display Units: % |
|
Steady Sequence Row |
SC, V |
Indicates the row of the sequence table that the module is moving towards. If the Sequence Table is not defined, this value is zero. |
|
System Enable |
Disables/enables the chiller plant. When System Enabled is False, the Chiller Selector downstages to zero capacity. |
False |
|
CHLR START DELAY (System Start Delay)b |
Indicates the delay applied when the System Enabled input transitions from Disabled to Enabled. The Minimum Load is maintained during this time allowing the chilled and condenser water pumps to operate. This time period is typically longer than the Stabilize Time to allow the system to achieve steady state after not being under control for some time. |
30 Display Units: Min |
|
Time Constant |
Indicates the amount of time required for a first-order system to reach 63% of its final magnitude, given a 100% step change of its process variable. The Period of execution of the module is Time Constant divided by 6. |
500 Display Units: Sec Range: 60-3,600 |
|
Total Current/Power |
V |
Indicates the total actual current/power output of all currently operating devices. |
0 Display units come from Current/Power Units. |
Tower Available Flow |
Indicates the available cooling tower flow based on tower enabled and its capacity. The Chiller Selector uses this value in determining valid device combinations. The value is typically available from the Cooling Tower Selector. |
0 Minimum Value: 0 Display units come from Flow Units. |
|
Tower Commanded Flow |
Indicates the Cooling Tower flow based on Cooling Tower status and its capacity. This value must be greater than the CW Min flow defined in the Device Info Table before the chiller can be commanded on. This value provides status feedback to the Chiller Selector to ensure proper sequencing of the cooling tower with the other equipment when a device is added or removed. The value is typically available from the Cooling Tower Selector. |
0 Minimum Value: 0 Display units come from Flow Units. |
|
Tower Piping |
Specifies whether operating with headered, dedicated, or no cooling tower piping on the Condenser Water side of the chiller. |
Headered Set Name: HeaderedDedicated |
|
CHLRx-UPPER PCT LOAD (Upper Optimal Pct Load) |
Indicates the right hand endpoint of the chiller efficiency plateau. When the percent load goes above this value, the module considers other combinations of devices that would produce a lower percent load. This is a nominal value that applies to the device individually. |
90 Display Units: % The minimum value must be greater than the Lower Optimal Pct Load value. Maximum Value: 100 |