The following table describes the attributes used by the Block Protect modules:
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Blocking On Time |
This input defines the duration of time to run the device. |
5.0 Seconds |
|
Command |
This input represents the command being sent to the device. |
Off Set Name: Off/On |
|
Max Off Time |
This output defines the duration of time between run commands to the device. If set to zero, blocking protection is not performed. |
7.0 Days Min Value: 0 Max Value: 45 |
|
State |
G |
This output displays Protect when the Max Off Time is exceeded and Command is Off. The device remains in the Protect state until Blocking On Time is met or the Command input is changed to On. |
Off Set Name: Block Protect |
Total Off Time |
SC |
This output indicates the amount of time spent in the Off state. When this value exceeds the Max Off Time input value the state switches to Run for the duration of the Blocking On Time. |
Display Units: Days |