Module Use in Applications (Subordinate Supply Flow Setpoint Control HFR) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use the individual modules in this group using the name in the following table.

Table 1. Subordinate Supply Flow Setpoint Control HFR Uses in Application System Selection Trees

Module Instance Name

Applications

Subordinate Supply Flow Setpoint Control HFR

VAV Subordinate Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.