Attributes (Subordinate Supply Flow Setpoint Control Dual Duct) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The following table describes the attributes used by the Subordinate Supply Flow Setpoint Control Dual Duct modules.

Table 1. Subordinate Supply Flow Setpoint Control Dual Duct Attributes

Name

Type 1

Description

Default Value

CD Percent

V

Flow setpoint rescaled between 0 and 100 percent. 0% maps to the min flow and 100% maps to max flow.

0.0%

CDFLOW-OUTSTATE, HDFLOW-OUTSTATE, or SAFLOW-OUTSTATE (State)

G, V

Current operational state of the output controller.

Min

Set Name: VAV DD Flow Controller

Deck Max Flow

 

Contains the maximum deck flow setpoint.

500 l/s, 1000 cfm

Deck Min Flow

 

Contains the minimum deck flow setpoint.

0 l/s, 0 cfm

Flow Percent

V

Flow setpoint rescaled between 0 and 100 percent. 0% maps to the min flow and 100% maps to max flow.

0.0%

Flow Setpoint

V

Contains the desired flow setpoint. This is the setpoint for another activity, typically the Supply Damper Control module.

0 l/s, 0 cfm

Mode

 

Contains the mode requested by State Selection.

Off

Set Name: VAV DD Flow Controller

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)