The following table describes the attributes used by the Application Mode Override module.
Name | Type | Description | Default Value |
---|---|---|---|
CD Min Flow | When the mode is set to Cool, the Minimum Cold Deck Flow Setpoint output is fixed at the CD Min Flow input value. When the mode is set to Auto, the Minimum Cold Deck Flow Setpoint output value varies from 0 to the CD Min Flow. When the mode is set to Heat, the Minimum Cold Deck Flow is set to 0. | 0.0 | |
CD Percent Cmd | The flow setpoint rescaled between 0 and 100 percent. A value of 0% maps to the 0 CFM and 100% maps to Min Cold Deck Flow. | 0.0 | |
Control Status | Current status of the controller. | Normal | |
Cooling Setpoint | When the mode is set to Auto, this setpoint indicates the zone temperature is near the cooling mode and needs minimum flow from the cold deck. | 74 °F, 23 °C | |
Eff CD Min Flow | Calculated min flow for cold deck. | 0.0 | |
Eff HD Min Flow | Calculated min flow for hot deck. | 0.0 | |
HD Min Flow | When the mode is set to Heat, the Minimum Hot Deck Flow Setpoint output is fixed at the HD Min Flow input value. When the mode is set to Auto, the Minimum Hot Deck Flow Setpoint output value varies from 0 to the HD Min Flow. When the mode is set to Cool, the Minimum Hot Deck Flow is set to 0. | 0.0 | |
HD Percent Cmd | The flow setpoint rescaled between 0 and 100 percent. 0% maps to the 0 CFM and 100% maps to Min Hot Deck Flow. | 0.0 | |
Heating Setpoint | When the mode is set to Auto, indicates the zone temperature is near the heating mode and needs minimum flow from the hot deck. | 70 °F, 21 °C | |
Min Absolute EWMA Effort | This value is an Exponentially Weighted Moving Average (EWMA). It is computed by the PID primitive and is based on the Current Present Value and the Last Present Value. It is the absolute value of the difference between the two. | 0.0 | |
Min Absolute EWMA Error | This value is an EWMA based on the absolute value of (Setpoint - Process Variable). | 0.0 | |
Min EWMA Error | This value is an EWMA based on the difference of (Setpoint - Process Variable). | 0.0 | |
Min EWMA Present Value | This value is an EWMA of the current Present Value. It is based on the difference of (Present Value - Last Present Value. | 0.0 | |
Mode |
|
Auto | |
PID Tuning Reset | Used to reset the tuning parameters for the PID. | Normal | |
Process ID | Used to configure the PID Pre-Processor. | °F, °C | |
State | State indicates the current operational mode of the output controller. | Min | |
Zone Temperature | When the mode input is set to Auto, the minimum flow setpoint outputs will be adjusted proportionally to the current temperature location in the dead band. | 72 °F, 22 °C |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)