Module Use in Applications (HD Constant Flow Setpoint) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The application System Selection trees in the software use the individual modules in this group using the name in the following table.

Table 1. HD Constant Flow Setpoint Uses in Application System Selection Trees

Module Instance Name

Applications

HD Constant Flow Setpoint Control

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.