The following table describes the attributes used by the HD Constant Flow Setpoint modules.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
CD Percent |
Contains a percentage that spans between the max and min flows. 0% maps to max flow and 100% maps to min flow. |
0.0% |
|
Deck Max Flow |
Contains the maximum deck flow setpoint. |
500 l/s, 1000 cfm |
|
Deck Min Flow |
Specifies the minimum deck flow setpoint. |
0 l/s, 0 cfm |
|
Flow Percent |
V |
Flow setpoint rescaled between 0 and 100 percent. 0% maps to the min flow and 100% maps to max flow. |
Display Units: % |
Flow Setpoint |
V |
Contains the desired Flow Setpoint. This is the setpoint for another activity, typically the Supply Damper Control module. |
0 l/s, 0 cfm |