Cascaded Zone Control - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Cascaded Zone Control output controllers provide a setpoint for another control loop (discharge air temperature or VAV flow control). The output controllers vary the setpoint based on the zone temperature and the appropriate zone heating or cooling setpoint.