Generic (Add New) Modules - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

For Custom Application creation, generic Network Inputs can be created using the right-click > New process available on the Network Inputs header in the Control View. You have the choice of creating a Boolean, Enum, or Float-based Network Input that can be renamed and integrated into the custom logic. See Adding a Network Input in the Configuring a System section.

The following table describes the generic Network Input modules and lists the applications in which they are used.

Table 1. Generic Network Input Modules

Name

Description

Applications

INPUT-BOOLEAN

CS Input (Boolean)

Custom Applications

INPUT-ENUM

CS Input (Enum)

Custom Applications

INPUT-FLOAT

CS Input (Float)

Custom Applications