Reliability (Unit Enable Determination ASC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Table 1. Unit Enable Determination Reliability

Input

Behavior When Input Is Not Reliable

Hardware Mode

Specifies that when Hardware Reliability is False, the State output matches the Network Mode if Network Reliability is True. If both Hardware Reliability and Network Reliability are False, the output is Enable.

Network Mode

Specifies that when Network Reliability is False, the State output matches the Hardware Mode if Hardware Reliability is True. If both Hardware Reliability and Network Reliability are False, the output is Enable.