Module Use in Applications (Unit Enable Determination - ASC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use the individual modules in this group using the instance name in the following table.

Table 1. Unit Enable Determination ASC Uses in Application System Selection Trees
Instance Name Application
Unit Enable Determination ASC

VAV Single Duct Applications

AHU Mixed Air Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.