The following table describes the attributes used by this module.
Name | Type 1 | Description | Default Value |
---|---|---|---|
Network Mode | Specifies whether to allow the unit to operate normally or shutdown.
|
Enable | |
Hardware Mode | Specifies whether to allow the unit to operate normally or shutdown.
|
Enable | |
Power Fail Restart Enable | When this value is set to true, a timer will hold the output at shutdown until the Power Fail Restart Time has elapsed. | False | |
Power Fail Restart Time | Sets the time to delay start when the power fail restart logic is enabled. | 60.0
Display Units = Seconds |
|
Resolution Mode | Used to determine how the input commands should be resolved into a single output command.
|
Either Can Shutdown | |
Restart Status | V | Indicates the status of restart for N2 compatibility. | False |
State | G, V | Current desired state for the unit.
|
Enable |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)