Device Types - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The N2 Mapping tab includes a Device Type setting. The following table shows the appropriate Device Type selection and corresponding controllers.

Table 1. Device Type Selection
Device Type Selection Applicable Controllers
AHU Generation 1 Application Specific (AS-AHU)
UNT Generation 1 Application Specific (AS-UNT)
VAV Generation 1 Application Specific (AS-VAV)
VND VMA1400, DX9100

All Other Controllers: DC9100, DCM, DR9100, LCP, MIG, NDM, PHX, TC9100, XT9100, XTM, XM1 (XBN), XM2 (XRM), XM3 (XRL or XRE), XM4 (XRL 2x2), XM5 (XRL 2x3), XM^ (XRM 2x2), XM7 (XRM 2x3)