Module Use in Applications - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This section indicates how the module is identified in the tool software. This section includes a table that lists the individual module instances used by that particular group of modules and the applications in which the module instance is used.

To see a module's connections and how modules interact with it, view the Connections table.