Miscellaneous Input Modules - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The Miscellaneous module category for inputs lists the miscellaneous inputs defined for the system. A miscellaneous input provides override monitoring. A miscellaneous input reads the current Present Value and Priority of position adjust outputPAO, analog outputAO, and binary outputBO objects.

See the following sections for information:

  • Applications: The application sections list the miscellaneous inputs used by a particular application.

  • Configuring a System: This section explains how to add a miscellaneous input, change a miscellaneous input name, and so on.

  • Commissioning a System: This section explains how to commission miscellaneous inputs.

  • Input and Output Objects: This section describes the objects used in the tool.

See the Upgrading System Files section for a list and description of the module and System Selection changes that were made since the last release of the tool.