Module Use in Application (MUX) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The application System Selection trees in the software use the individual modules in the following table.

Table 1. Module Use in Application (MUX)

Module Instance Name

Applications

CPO-30 Enable Switch

Central Cooling with Optimization Applications

CPO-30 Cap Limit Switch

Central Cooling with Optimization Applications

CPO-30 Cooling Mode Output

Central Cooling with Optimization Applications

CPO-30 CWP Ramp Time Switch

Central Cooling with Optimization Applications

CPO-30 PCHWP Ramp Time Switch

Central Cooling with Optimization Applications

CPO-30 SCHWP Ramp Time Switch

Central Cooling with Optimization Applications

CPO-30 TWR## Run Switch

Central Cooling with Optimization Applications

Hx CPO-30 Enable Switch

Central Cooling with Optimization Applications

WSE Chiller Selector Enable Switch

Central Cooling with Optimization Applications

WSE Hx Selector Enable Switch

Central Cooling with Optimization Applications

WSE Tower Enable Switch

Central Cooling with Optimization Applications

WSE Chlr CHW Current Cap Switch

Central Cooling with Optimization Applications

WSE HX CW Current Cap Switch

Central Cooling with Optimization Applications

Hx CW Pump Capacity Check

Central Cooling with Optimization Applications

WSE CW Pump Count LV Switch

Central Cooling with Optimization Applications

WSE Pump Startup Reqd

Central Cooling with Optimization Applications

WSE CW DP Setpt Switch

Central Cooling with Optimization Applications

WSE CW-T Setpt Switch

Central Cooling with Optimization Applications

WSE Twr CS State Switch

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.